Go to description Go to description Go to description Go to description Go to description Go to description

General (Basic LTE-A Pro FDD PRACH)

This topic describes the General parameters for the various Basic LTE-A Pro PRACH component carrier types, including E-UTRA, eMTC, and NB-IoT.

The Baseband parameters are described in Baseband (Basic LTE-A Pro PRACH).

State

Double-click or use the drop-down menu to turn the carrier Off or On.

Waveform Generation Length (E-UTRA & eMTC)

Range: 0.1 or 1 to 1024 frames

Step: 1 frame (10 ms)

Default: 1 frame (10 ms)

Sets the waveform generation length. When the parameters are set by PRACH Wizard, the waveform generation length is automatically set to the appropriate value.

Waveform Generation Length (NB-IoT)

Range: 40 to 40960 ms

Step: depends on NPRACH Resource Periodicity in Channel Setup node

Default: 80 ms

Sets the waveform generation length.

Waveform Generation Length must be a multiple of NPRACH Resource Periodicity on “Channel Setup” node and the input value is rounded up to the nearest multiple of NPRACH Resource Periodicity.